Part Number: SN65HVD11
hi dear supporting team,
as for SN65HVD11D, because it is at the brd edge which interface to external, if in lightening stroke, suppose the A/B prot pin is shorted to GND, could we gurantee the shorted current to GND be smaller than 50mA over whole temp range? if it is exceed 50mA, is there any internal protection that could shut it off, and when the shorted case is passed, then it could recovered itself? tks a lot!