This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RS485 terminal resistor select



Hi TI,

How to decide the resistor in the RS485 receiver?And its power and value?

Best regards,

Frank

  • Hi Frank,

    The termination resistors on the RS-485 bus should match the cabling characteristic impedance value, which typically is 120ohm.  Having two terminations on the bus will put a 60ohm load on the bus, which is typical.  

    In normal operation, RS-485 drivers will drive a maximum of 5V differential signal onto the bus lines, which create a P=V^2/R power dissipation value of 25/120 = 208mW.  

    Therefore, a 0.25W rated resistor will work for normal operation; however, during a fault condition on the bus, the power dissipation may rise to higher levels.  The worst-case fault condition would occur if one bus pin is shorted to -7V and the other bus pin is shorted to +12V.  Under these extreme voltage conditions, the power dissipation could rise to 19*19/120 = 3W.

    Choosing termination resistors at 3W is pretty extreme.  Usually a system designer will choose a trade-off with bus fault conditions and lower power-rated resistors.  If you choose to protect against a single pin shorting to -7V or +12V individually, then you could choose a resistor in the 0.5W to 1.5W range.  

    Does this information help?  Please let me know if I can help answer any more questions you have.

    Best Regards,
    Max Megee

  • Hi MAX,
    Thanks a lot.Can you give me some typical RS485 application circuits to understand your nice replay.I want to know why the bus pin can be shorted to -7V,how does it occur?
    Best regards,
    Frank
  • Frank,

    One of the advantages of the RS-485 interface is the ability to tranfer data over long distances with large ground potential differences (GPD) between nodes.  This is the reason that the RS-485 standard specifies transceivers that operate across a common mode range from -7V to 15V.  If it happens that one of the bus lines are shorted to ground or supply, then this common mode voltage short can create the large amplitude fault condition.  The figure that I have attached below offers some advice on proper grounding techniques to reduce ground loop currents when GPD is high.  I include it here just to show how ground potential differences can contribute to higher voltage fault conditions in RS-485.

    Does this make sense?

    Regards,

    Max