Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD1452: RS-422 / RS-485 Full Duplex with Switchable Termination in a multi-protocol context

Part Number: THVD1452

Does TI offer any RS-422 / RS-485 full duplex drivers incorporating switchable 100Ω or 120Ω termination? Something >= 5Mbaud with DE, nRE and optional slew-limitation like the LTC2861.

This in order to construct a multi-protocol buffer in a fashion similar to that described in TI's tidua80 document. The device should therefore be able to handle 1Mbaud 232 levels on the line interface side when disabled, ideally not loading the line in this state.

The THVD1452 seems a possible candidate but has no switchable termination. Any suggestions to otherwise implement switchable RX termination in an elegant fashion?