Other Parts Discussed in Thread: TPS65987D, , HD3SS460, TUSB1064
Hello,
I'm trying to make a HUB circuit, with a full-featured USB Type-C as my Upstream port and, for Downstream, one full-featured USB Type-C port and a USB 3.0 Type A port. I've decided to use a TUSB8044 as the HUB circuit and the TPS65987D as the PD Controller, and I have been studying and figuring out almost everything, but I'm having issues with some connections.
1) As described below, I'm not getting exactly how to manage the SBU ports of both the Upstream and the Type C Downstream (See the picture below). Since I want a full-featured type C Downstream, I believe I need to connect both SBU ports from the Upstream connector to the Downstream one. Is this correct? The TPS65987D does not have any connections for SBU...
2) I'm only using 2 of the TUSB8044 Downstream ports, but I'm not sure what to do with the other 2 DFP. Can I leave them not connected? Does it need to be pulled up/down?