Part Number: TRSF3238E
Other Parts Discussed in Thread: TRS3238E, MAX3238E, MAX3238
I'm using a TRSF3238E in a low-speed interfacing application, where the '32328E is continuously transmitting data (RXD) to a DTE on pin 12 (Dout5) while listening for RTS from the DTE on pin 11 (Rin3). Dout5 is driven even at times when the DTE is disconnected or the Rin3 pin is tri-stated.
While testing this circuit I noticed noise spikes on the Rin3 pin, coincident with the rising and falling edges on Dout5. With cables disconnected from my board these spikes are about +/-1V. With a 10ft cable connected to my board the noise spikes exceed +/-2.5V and the '3238E acts as if it is receiving valid RTS pulses on Rin3, even though the terminal at the other end of the cable is turned off.
- I've reviewed my PCB artwork and the trace spacing is sufficiently large that I wouldn't expect coupling between Dout5 and Rin3 on the board.
- My design uses 0.22uF caps, as recommended for a 3.3V design
- FORCEON and /FORCEOFF are always high
Are there any failure modes that could explain the RIN pin being driven?