Part Number: TUSB1002
Dear Technical Support Team,
I have a question about "Changes from Revision A (May 2016) to Revision B".
This was updated about RXP2 and RXN2 like adding capacitor and pulldown register.
What is the background of this changes?
I think that some connection is failed without capacitor for AC coupling and pulldown register(DC coupling).
So is it recommended from DC coupling to AC coupling,right?
■Changes from Revision A (May 2016) to Revision B Page
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------
• Added a capacitor to the RXP2 and RXN2 pins of the Simplified Schematic........................................................................ 1
• Added a capacitor to the RXP2 and RXN2 pins of Figure 17 .............................................................................................. 19
• Updated the A/C coupling Capacitor section of Table 4 ..................................................................................................... 19
• Changed text in the Detailed Design Procedure From: No A/C coupling capacitors are placed on the RX2P/N. To:
330nF A/C coupling capacitors along with 220k resistors are placed on the RX2P and RX2N. Inclusion of these
330nF capacitors and 220k resistors is optional but highly recommended. If not implemented, then RX2P/N should
be DC-coupled to the USB receptacle. ................................................................................................................................ 20
• Added 330nF AC capacitors (C12 and C13) on RX2P and RX2N in Figure 18 .................................................................. 20
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Best Regards,
ttd