Part Number: PCA9306
Other Parts Discussed in Thread: TCA9406, LSF0102, TXS0102
Dear Team,
I have two questions about PCA9306 as below.
1. I want to know is SW a pure Mosfet in PCA9306? Is there any other control logic in PCA9306 (like one-shot circuit in TCA9406) ?
2. Patrick showed below figure and illustrated the concept of the high bit pass from the host to the slave in another E2E thread.
But I have a question that will it has reverse current from 3.3V to 1.8V? Is our switch Hi-Z also when high bit pass?
Thank you.