Part Number: TPS65987D
Other Parts Discussed in Thread: TIGER
1. May I know the schedule of next patch after F707.10.05?
2. Customer want to know detailed HRESET description and ask to add into datasheet, please help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tiger,
Patch F707.10.06 was released today, you should see it available soon.
toggling the HRESET pin will force a reboot of the device similar to the Gaid command. This will cause the Cortex M0 to reboot. If there is a valid configuration available in RAM, it will reload that configuration and not reload from the SPI Flash.
If this answers your question, PLEASE select This resolved my issue
Thank you,
Eric
Thanks Eric.
Sure, I had received F707.10.06 patch.
For HRESET, customer is asking to add into datasheet, please help.