Part Number: AM26C32
Hi All
My customer is considering to use AM26C32 for their 3ch RS422 application.
Then, how should they handle unused pins ?
for example :
- Output = Pin #13
- Input = Pin #14, #15
Please advice
Best regards,
HIRO
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello HIRO-san,
It is OK to leave unused output and input pins disconnect (floating) on this device. If you wanted to reduce the chance that the unused channel toggles (i.e., based on noise present at the input), then you could use a pull-up resistor on one input line and a pull-down on the complementary input. Typical values would be 1 kOhm to 10 kOhm.
Max