Part Number: DS90UB954-Q1EVM
Other Parts Discussed in Thread: DS90UB953-Q1EVM, , ALP
Hello TI,
I am working on a demonstration using your DS90UB954-Q1EVM and DS90UB953-Q1EVM kits. The 953 also comes with a CSI-2 imaging sensor which uses 4 CSI-2 data channels. Both kits use all 4 data channels (D0, D1, D2, and D3) per the schematics. Is it possible to display an image through a basic Raspberry PI. A Raspberry PI has a CSI-2 input connector, but only uses 2 data channels rather than 4. I want to use a Raspberry PI since I have a Raspberry PI DSI display setup already. Would this work? If not, how can I easily access and use the CSI-2 data from J24 connector on the 954 demo board to display the image from the 953 eval kit? Thank you!
Emilio