Part Number: DS90UB964-Q1
Other Parts Discussed in Thread: ALP
Hi
I am trying to enable the pattern generation feature in DS90UB964-Q1 in our SoC. I am running the following script :
# 1920*1080 @ 30 fps
# 4 x lane 800Mbps/lane
# Data Type: RAW12
# Data
#
# Hactive:1920 pixles
# Vactive:1080 lines
# Vtotal:1125 lines
# Vfront:10 lines
# Vback:33 lines
# Pixel size: 12 bits (Mipi CSI-2, Table 25 )
# Block size: 3 bytes (Mipi CSI-2, Table 25 )
# Frame rate: 30 fps
# Number of bars: 8
#
# Reset
i2cset -f -y 6 0x30 0x01 0x01
# Set CSI_TX_SPEED to select 800Mbps
i2cset -f -y 6 0x30 0x1F 0x02
#
#
# CSI sel and CSI enable
i2cset -f -y 6 0x30 0x32 0x01 # CSI0 sel and CSI0 enable
i2cset -f -y 6 0x30 0x33 0x03 # CSI_LANE_COUNT: 4, EN Continuous Clock
i2cset -f -y 6 0x30 0x20 0x30 # Disable video forwarding by setting bits [5:4] of the FWD_CTL1 register
i2cset -f -y 6 0x30 0x21 0x80 # Enable CSI Replicate Mode
# enable pat gen
i2cset -f -y 6 0x30 0xB0 0x00 # Indirect Pattern Gen Registers
i2cset -f -y 6 0x30 0xB1 0x01 # PGEN_CTL
i2cset -f -y 6 0x30 0xB2 0x01
i2cset -f -y 6 0x30 0xB1 0x02 # PGEN_CFG
i2cset -f -y 6 0x30 0xB2 0x33 # NUM_CBARS, Block_size
i2cset -f -y 6 0x30 0xB1 0x03 # PGEN_CSI_DI
i2cset -f -y 6 0x30 0xB2 0x2C # RAW12 Data Type
i2cset -f -y 6 0x30 0xB1 0x04 # PGEN_LINE_SIZE1: 1920*12/8=2880
i2cset -f -y 6 0x30 0xB2 0x0B
i2cset -f -y 6 0x30 0xB1 0x05 # PGEN_LINE_SIZE0: 1920*12/8=2880
i2cset -f -y 6 0x30 0xB2 0x40
i2cset -f -y 6 0x30 0xB1 0x06 # PGEN_BAR_SIZE1: 1920*12/8/8)=360
i2cset -f -y 6 0x30 0xB2 0x01
i2cset -f -y 6 0x30 0xB1 0x07 # PGEN_BAR_SIZE0: 1920*12/8/8)=360
i2cset -f -y 6 0x30 0xB2 0x68
i2cset -f -y 6 0x30 0xB1 0x08 # PGEN_ACT_LPF1: 1080
i2cset -f -y 6 0x30 0xB2 0x04
i2cset -f -y 6 0x30 0xB1 0x09 # PGEN_ACT_LPF0: 1080
i2cset -f -y 6 0x30 0xB2 0x38
i2cset -f -y 6 0x30 0xB1 0x0a # PGEN_TOT_LPF1: 1125
i2cset -f -y 6 0x30 0xB2 0x04
i2cset -f -y 6 0x30 0xB1 0x0b # PGEN_TOT_LPF0: 1125
i2cset -f -y 6 0x30 0xB2 0x65
i2cset -f -y 6 0x30 0xB1 0x0c # PGEN_LINE_PD1:1/(30*1125*10ns)=2963
i2cset -f -y 6 0x30 0xB2 0x0B
i2cset -f -y 6 0x30 0xB1 0x0d # PGEN_LINE_PD0:1/(30*1125*10ns)=2963
i2cset -f -y 6 0x30 0xB2 0x93
i2cset -f -y 6 0x30 0xB1 0x0E # PGEN_VBP: 33
i2cset -f -y 6 0x30 0xB2 0x21
i2cset -f -y 6 0x30 0xB1 0x0F # PGEN_VFP: 10
i2cset -f -y 6 0x30 0xB2 0x0A
DS90UB964 has been configured for RAW 12 HF, Coax mode. I2C address is 0x30(7-bit) and 0x60(8-bit).
But I am not seeing any change in registers 0x73-0x76. i2cdump result after executing the script:
$ i2cdump 6 0x30
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 60 00 1e 30 c2 01 00 fe 1c 10 79 79 0f b9 00 ff `.?0??.???yy??..
10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 04 02 ..............??
20: 30 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 0?..............
30: 00 00 01 03 00 00 00 00 00 00 00 00 00 00 00 00 ..??............
40: 00 a3 01 01 00 00 00 00 00 00 00 00 00 00 02 00 .???..........?.
50: 00 00 00 00 00 00 00 00 18 00 00 00 00 00 00 00 ........?.......
60: 00 00 00 00 00 00 00 00 00 00 00 00 00 7e 88 88 .............~??
70: 2b 2c e4 00 00 00 00 c5 00 01 00 00 20 00 00 00 +,?....?.?.. ...
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
b0: 00 0f 0a 08 25 00 18 00 8e 03 03 74 80 00 00 00 .???%.?.???t?...
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
d0: 00 43 84 27 60 f8 07 00 00 00 00 00 00 00 00 00 .C?'`??.........
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
f0: 5f 55 42 39 36 34 00 00 00 00 00 00 00 00 00 00 _UB964..........
Can anyone suggest what could be the problem?
Regards
Sneha