Part Number: SN65DSI86
SN65DSI86 support team
I have two questions:
1. The panel specification that customer uses is as follows
- Resolution = 2048 x 1536
- Refresh Rate = 60Hz
- DP I/F = 2.7Gbps (HBR)
How many lanes should they use for DSI between SoC and SN65DSI86l?
2. The datasheet is mentioned as follows :
How much is the specific loss at above condition ?
Customer need to use not FR4, but micro-coax cable which the length is 20cm. They would like to estimate the total loss in considering a micro-coax cable.
Note. the below is a guidelines of a micro-coax cable shown by Intel.
Thanks
Tamio