This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD1E05U06-Q1: Protection of USB 2.0 Lines fails

Part Number: TPD1E05U06-Q1

I am using the TI TPD1E05U06-Q1 TVS to protect my USB 2.0 DP & DN lines that are connected to a FTDI FT601 chip and the the communication is failing. I measured approx 800mV on the DP and close to 0V on the DN lines. When I removed the TPD1E05U06-Q1 the communication worked. I checked carefully the connections and ensured that PIN-1 is connected to the I\O and PIN-2 is connected to GND for both signals ! I re-soldered new components and it didn't help. Also we are seeing this effect in multiple devices on different computers ! 

Please could someone help me with this ?