TCAN4550-Q1 team,
The datasheet section 9.1.1 says the crystal or clock should be a minimum of 20 MHz, while 40 MHz is recommended for CAN FD. Is it the case that 20 and 40 Mhz are the only options, or can other frequencies be used within that range?
The customer doesn't need to reach FD rates, just 1 Mbps max.
I noticed the Watchdog register only allows a choice or 20 or 40 MHz, but the precision of the watchdog is probably not so important.
Thanks,
Darren