Hi Team,
The customer has below issue need your help.
Question:
TVP5151 uses PAL mode, the color is not normal in the color bar test.
The configuration method is to use example1 in the manual.
status register #1 0x88 ==> 0x6e
status register #2 0x89 ==> 0x18
status register #3 0x8a ==> 0x15
status register #4 0x8b ==> 0x20
status register #5 0x8c ==> 0x83
Thanks.