Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
Hi Team,
"TPS65987DDH Host Programming for SPI-Flash Less Systems" Application Report: SLVA972–May 2018
On page 6, 3.1.2 Execution Flow, Section 2, there is the following description,
"1. The device generates an I2C event, READY_FOR_PATCH, indicating that it is ready for patch. The
host shall start the patch download process after receiving this notification from the device "
Q1:Is the I2C event READY_FOR_PATCH necessary? I found when my BusPowerZ Configurations is
| BP_ECWait_External | Infinite Wait |
and read 0x03 Mode register, the mode is "PTCH", read 0x14/15 intEvent1/2, the bit ready for patch is 0.At this status, can the host download the patch bundle to TPS65987?
Q2: before download patch bundle, which mode should be in mode register?APP or PTCH? I'm not sure what "PTCH"mode means.
"NOTE: If the host intends to load a different patch bundle (either apllication configuration and/or
device patch) after the device has already transitioned to the 'Application' mode (either by
loading the default configuration or after a previous patch download sequence), the above
patch download sequence shall be preceeded by a 'PTCr' (Patch Reset) and succeeded by a
'Gaid' (Warm Restart) 4CC command. "
Q:does the sequence look like this: PTCr->Gaid->patch download sequence, or PTCr->patch download sequence->Gaid, which one is right?
Best Regards,
peng