This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD6S300: when CC Short-to-VBUS through a cable,during the ringing the maxium voltage can be up to 44V ?How do you get 44V?

Part Number: TPD6S300

  On page 6 of  the  documnet "Circuit protection for your next USB Type-C™ design White Paper  " says ,when CC Short-to-VBUS through a cable,during the ringing the maxium voltage can be up to 44V ?How do you get  44V? 

  Below is the detailed description,but I still can't  understand that,need your help!!!  

  As the waveform shows, when a cable is present during a short-to-VBUS event, enough inductance exists in the resistor-inductor-capacitor (RLC) circuit relative to the resistance and capacitance to generate a peak voltage during the ringing that is nearly double the value of the settling or final voltage. If the CC line capacitors de-rate greatly over their voltage range, then the peak voltage that is present during the ringing can be more than double the setting or final voltage. This means for a 22-V short, up to 44 V can be seen on the CC or SBU lines during a short-to-VBUS event. What was initially thought to require only 22-V protection ends up needing to be 44 V.

  

Thanks~