Part Number: TCA5013
Dears,
we are pushing TCA5013 for smart phone, the customer has some issues as below:
1. how to connect the D9(CLKIN1),F9(CLKIN2),E8(IOUC_1),F8(IOUC_2) with the controller? is it I2C Bus alike?
2. how to connect D9(CLKIN1),E8(IOUC_1) pins if the user card is not employed? pull them to GND or just let them floating?
3. what type of user card does TCA5013 support? only SMART CARD?
4. has TCA5013 been employed with MTK mobile phone platform? what Android version may TCA5013 support?
5. If the ISO7816 protocol been built-in the driver code?
thanks!