Part Number: DS90UB964-Q1
Dear team,
My customer test 964 with two different cables(dacar 302 cable and RG 174 cable) using MAP tool. When the cable is 2 meters, the dacar 302 cable's result is worse than RG174 cable, which is abnormal.(Because the dacar 302 cable's performance is better than the RG 174 cable). Could you please tell me the reason?(The first picture is dacar 302, and the second picture is RG 174)
When the cable is 5 meters, the results are similar. First picture is dacar 302, and the second picture is RG 174.
In addition, now you recommend the customer to use MAP tool, in this way, they need to use the manual EQ instead of AEQ. But when the cable has been used several years, the fixed EQ value is also available for this cable?
Third question, this inface includes two parameters: EQ & SP. I can change EQ value through the register, but I don't know how to change SP because I don't find any related register. Could you please tell me how to change SP?
Thanks & Best Regards,
Sherry