This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you please kindly suggest if TI best solution to replace ISL83080EIBZ-T on RS-485/RS-422 Transceivers.
Thanks a lot!
Best Regards,
Sean Liao
Hi Sean,
Do you need a pin-for-pin drop-in device? If so I'd recommend looking at THVD1452. It uses the same package and footprint but supports a wider VCC range, larger output voltage (useful for longer distances), and has enhanced ESD performance (+/- 18 kV IEC 61000-4-2 contact discharge).
Please let us know if you have any questions or feedback related to this device.
Regards,
Max