Part Number: TVS3300
Other Parts Discussed in Thread: LM53635-Q1,
Hi,
I am using LM53635-Q1 DC/DC converter to generate 5V system power supply from +24V automotive battery. Absolute maximum rating for input voltage on LM53635-Q1 is +40V, so using the conventional 33V TVS would not protect it given that clamping voltage is >45V. Using TVS with lower voltage is not an option because it would affect the normal operation conditions.
I believe TVS3300 would be a good alternative for conventional TVS.
Do you see any problem in using TVS3300 for +24V/1A input power line or, alternatively, do you have any other suggestion?
Thanks,
Goran