Part Number: TCAN4550-Q1
Hello,
I have a question about Under Voltage Threshold.
[Q]
Recommended Operating Conditions Vsup = 5.5~30 [V]
UVsup(Under voltage detection on VSUP rising ramp for protected mode) = 5.9 [V](max)
Does this mean that TCAN4550-Q1 may not work properly when used at Vsup = 5.5V?
*Background to this question
- My customer is considering using Vsup = 6V.
- The accuracy of the power supply that generates 6V is ± 3%.
- The worst value of the power supply is 5.82V.
- At this time, may TCAN4550-Q1 not operate by UVLO?
Best Regards,
Kaede Kudo