Part Number: SN65CML100
Hi,
I would like to use SN65CML100 to convert LVPECL to CML as below figure shows. Where should I add the termination resister for LVPECL?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65CML100
Hi,
I would like to use SN65CML100 to convert LVPECL to CML as below figure shows. Where should I add the termination resister for LVPECL?
Thanks.
Jerry
If you are driving a LVPECL input, you would need 50-Ω resistors on both A and B to a termination bias voltage, VT. VT is usually 2-V below the supply voltage of the driver circuit. When the driver operates from a 3.3-V supply, VT is set to approximately 1.3 V.
Thanks
David