This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Nicky,
Yes LMH1219 IN1 100-ohm differential input does support SMPTE. Please note we need to use either SMBus or SPI interface to setup the registers as noted below:
RAW FF 05 07 //Enable EQ core
RAW 31 20 30 //Power up OUT0
RAW 33 20 30 //Power up OUT1
RAW FF 04 07 //Enable lmh1218 core
RAW 3F 04 04 //Override reference rate
RAW 2F 00 C0 //Enable CDR lock to SMPTE rates
RAW 3F 10 10 //Override IN_OUT_SEL pin
RAW 31 03 03 //Select IN1 to OUT0 and OUT1
RAW 3F 08 08 //Override OUT_CTRL
RAW 09 00 20 //Disable independent output control
RAW 1C 08 0C //If locked OUT0/1 reclocked data else raw data
RAW 0A 0C 0C //Reset CDR
RAW 0A 00 0C //Release Reset
Regards,, Nasser