Hi Team,
Do we have a TI product to recommend with the customer with something like SN75LBC968 but can interface between 5V TTL BNC cables and 1.2V logic to FPGA on PCB.
The customer application was to drive 75-ohm BNC cables at up to 100Mbps with the bidirectional performance provided the control voltage is 1.2V logic. The component must also interface between 1.2 V logic in the controller and 5V logic in the BNCs.
Another device he needs is for the same application but for >200Mbps differential +/-5V RS-422 Tx/Rx to 1.2V LVDS.
Please let me know if you need more information.
Thanks!
Jonathan