Part Number: SN65DSI86
Hello,
one of my customer is searching for MIPI-to-eDP solution and the spec requirements from system as below ; can SN65DSI86 meet them? or do we have a better product to suggest?
===============================================
1. Resolution : FHD@60Hz
2. Input I/F : mipi 4-lane
3. Output I/F : eDP 2-lane @ HBR (2.7Gbps)
4. ASSR support
5. Dimension : small size is preferred
6. Power consumption : low power consumption is preferred
7. Special Feature : MIPI M/N value auto setting (H/W or F/W) - not manual setting
detail about no. 7 : there are multiple MIPI sources as input interface so, the driver should automatically detect & adjust the M/N value of MIPI clock accordingly. it should be HW or FW controlled, not by manually software.
=======================================================================
Can SN65DSI86 support what customer needs ? ?
Thanks in adv.