Other Parts Discussed in Thread: TCAN332, SN65HVD233
Can TCAN332G communicate with SN65HVD233DR?
At present, CTM old product CAN socket is sn65hvd233dr, and the new one they want use is tcan332g which supports FD.
When using 500kbps rate, CAN the new and old device communicate normally? (physical connection interface has been confirmed and supported)
According to datasheet, there is a difference of 0.45v in the Recessive level between the two chips. TCAN3323G is 1.85V and SN64HVD233 is 2.3V
Will it cause chip damage? What is the output structure of CANH\L pin?