Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: , DS90UB914A-Q1, DS90UB913Q-Q1
I'm attempting to see if I can use the DS90UB953-Q1 serializer with the DS90UB914-Q1 deserializer, as described in SNLA270 (which refers to the DS90UB914A-Q1). I'm bench prototyping this using the DS90UB953-Q1EVM, connecting via twisted pair to the DS90UB914-Q1 on our existing hardware. I get a good LOCK output from the DS90UB914-Q1, suggesting that the FPD-Link III channel is working, and the I2C address of the DS90UB953-Q1 shows up in the SER ID register (0x06) of the DS90UB914-Q1. I copy the 953's I2C address from the SER ID register to the SER Alias register (0x07), but then when I try to access the '953, the '953 apparently initiates a really long clock stretch, eventually forcing the I2C master behind the '914 to give up:
Is this a compatibility difference between the DS90UB914-Q1 and the DS90UB914A-Q1 that will prevent the "non-A" version from working with the DS90UB953-Q1?