This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401A-Q1: Analog input common mode voltage range issue

Part Number: TFP401A-Q1

Hi team,

Customer tested two input, one has a common mode level of 2.91V measured at the TFP401 input, and another has a common mode level of 3.05V measured at the TFP401 input, 
and AVDD = 3.3V.
1. What is the risk when common mode resonance does not meet the chip requirements? What are the undesirable consequences?
2. What is the probability of risk?
3. Does the chip have an interface to adjust the common mode?
4. Could customer adjust the AVDD to 3.0V? Thanks.
  • Hi Jeff,

    1. The risk is the device not operating as intended, as is the case when operating outside of datasheet specifications for all specs 

    2. This has not been quantified

    3. The chip does not have an interface to adjust the common mode

    4. Yes, as 3V is within datasheet specifications

    Regards,

    I.K.