Other Parts Discussed in Thread: BQ24380, BQ24351, BQ24308, BQ24350
Hi Team,
Here is a requirement as below. EE is smartphone. The device will be put before charger.
Vin=2.8~12V, absolute value is 28V, has OVP function, integrated Rdson is below 55ohm, Iout is 4.5V. single channel.
System ESD test: IED61000-4-2, contact >=8kV, air >=15kV.
Please kindly check if there is proper device. Thanks.
BRs
Given