Part Number: TUSB1002
We need to verify our design from a low level. The tusb1002 sits on board with a connector (COM-express) towards the CPU module, and a pinrail connector towards a USB "pigtail" for chassis mount.
Things are routed in 85Ohm differential, also around the connectors. We are though having troubles and wants to verify end to end using a (2-port)-VNA 8GHz, and the question to you is is that a possible way to go?
Do you have any suggestions for debugging besides using expensive Oscilloscopes and BER testers, eventually using the VNA ?
Do the tusb1002 train its equalizer on the USB bit sequences ?