This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We would like to use INTB to tell the SOC that HDMI hot plug are detected.
Besides setting register 0x54 bit 6 =1 and register 0xC6 bit 0 = 1.
Any other setting is needed ?
Hello PYT,
You need also to enable global interrupt in reg 0xC6[0].
Hi Hamzeh,
Do i need to connect DS90UH949-Q1 to a deserializers like DS90UH940-Q1/DS90UH948-Q1 to make this function work ?