Part Number: TCA6424A
Hi,
I have a question about TCA6424A address setting. If VCCP is 1.8V, can we use 3.3V at ADDR pin? From data sheet, "H" level requests 0.7Vccp ~ 5.5V.
Is it OK to set "H" in address? It's a 2nd source replacement question.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA6424A
Hi,
I have a question about TCA6424A address setting. If VCCP is 1.8V, can we use 3.3V at ADDR pin? From data sheet, "H" level requests 0.7Vccp ~ 5.5V.
Is it OK to set "H" in address? It's a 2nd source replacement question.
Hey Alan,
I looked under the hood at the address pin for this device and found an ESD cell in series with a CMOS gate. The ESD cell should have no problems with this as long as you don't drive the input of the address pin below GND or above ~7V. The CMOS gate should be okay with this as well as long as you don't violate the absolute maximum conditions.
-Bobby
Hi Bobby,
Another question is ADDR pin pull-high timing. Any timing request? example:
1. if 3.3V is 1st coming, then VCCP is ready?
2. if VCCP is ready, then 3.3V is available.
When does device detect ADDR pin voltage level and decide address?