Part Number: AM26LS32A
Q-1: I want to convert 1 volt Peak to peak sinusoidal voltage input to 5V square pulse. Can I use AM26LS32A:Quadruple Differential Line Receiver for the same purpose ?
Q-2: If It can not be used, then why?
Q-3: AM26LS32A can only be used for differential quadruple input (square pulse) or can be used for peak to peak sinusoidal differential input signal also??