Part Number: SN65HVD75
I'm using the SN65HVD75 with the REnot and DE tied together. In the specification it claims that Transmitter takes 3usec typical to enable if receiver had been disabled, otherwise it only takes 10nSec typically. I don't understand the reference to Receiver enabled or disabled. SO like I've said I tie the REnot and DE together so I suppose the receiver is momentarily disabled. In my situation do I need worry about the 3-7uSec Driver enable times tpzh and tpzl?
Likewise for the "Receiver enable time" do I need to worry about the 3 to 8uSec specifications when tying REnot and DE together.
Under what conditions do the longer enable times for the receiver or transmit driver come into play?