Part Number: DP83867IR
Hi team,
With a link up with a link partner at a media speed of 100M Full Duplex, our board links down once every few hours. The link partner side does not link down.
As a result of evaluation with 3 measuring instruments and 1 personal computer, 2 measuring instruments (same model) will be linked down.
The difference between link down and not link down is the content of bit [12: 8] in register 0x002D.
① Link down
0x002D [12: 8] = {0,0,01,1,0}
Enable FLD (0x002D, bit [15] = 1) in this state, link down immediately
② Not Link down:
0x002D [12: 8] = {0,0,01,1,0}
In this state, Enable FLD (0x002D, bit [15] = 1), no link down
Question 1: Conditions for detecting and canceling Bit10 (MLT3 Error)
Question 2: Conditions for detecting and canceling Bit9 (SNR level)
Question 3: Conditions for link down in the normal state (0x002D bit15 = 0)
A) Does the link down condition differ depending on FLD on / off?
B) The conditions are the same, but the threshold is different?
C) etc.
//
Thank yo.
Best Regards,
Ryo Kukita