Part Number: SN65ELT20
Hi all,
I have a problem with SN65ELT20 part. The problem is not with the part itself but I am looking for a suitable replacement with the same pinnout but apart from the PECl logic at the output I am looking for the part with the clasicc 5V TTL/CMOS diff logic at the output. It is cause of the compatibility with the older device and I do not want to create a new board design or any additional boards to put in between. Thanks a lot for any feedback.
Kind Regards
Ondrej