Other Parts Discussed in Thread: TPS2041C, TPS2051C, , TPD6E05U06, TS5USBC41, TPD4S311
Hi Team,
I have a question about USB DPR.
Here is requirement for USB and i'm looking for what is the best solution for it.
[Requirement]
USB cable: USB type-C
USB data: USB2.0
DFP/UFP/DPR: DRP support
Power: source 5V/500mA during host/DFP. no sink during slave/UFP.
Question here is
- can below figure achieve above requirement?
- depending on ID pin state, processor has to change the state of host or slave?
- are there any concern about below figure?
- are there any other recommendation for above requirement?
- default initial value at startup is 500mA so no need to setup anything for USB2.0 current setting?
Regards,
Kai