This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS181: TMDS181: No signal output when configured via i2c mode

Part Number: TMDS181


Hi ,all,

Using TMDS181RGZT and TPD12S016RKTR to build the HDMI signal channel between FPGA and display (FPGA is the sending end and the display is the receiving end).

The current problem is: HDMI don't output to 4K or 1080P via i2c mode ,but HDMI signal can display via pin strap mode.

Do you have any suggestion why TMDS181 don't have output via I2C mode?

7776.I2C register dump.TXT0312.TMDS181-OUTPUT-SCH.pdf

  • Hi,

    There are couple issues I see in the schematic.

    1. SDA_SRC and SCL_SRC need to be pulled to ground if not used

    2. SDA_SNK and SCL_SNK need to be connected to the DDC bus between the FPGA and the HDMI connector so the TMDS181 can snoop the DDC bus and correctly set the TMDS_CLK_RATIO_STATUS bit

    3. Are you connecting the HPD signal from the HDMI connector to the FPGA?

    4. How does the OE pin being controlled? The OE pin has an internal pullup so it only needs an external pulldown capacitor. We recommend a 0.22uF cap on the OE pin to make sure the power up timing requirement can be met

    In the register dump, I see the TMDS_CLK_RATIO_STATUS being set to 1. TMDS_CLK_RATIO_STATUS only sets to 1 for HDMI2.0, it needs to be set to 0 for HDMI1.4 or lower operating speed.

    Thanks

    David

  • Hi,David

     Thank you for your reply!

    1、SDA_SRC and SCL_SRC  have been pulled to groud;

    2、SDA_SNK and SCL_SNK have been connected to he HDMI connector,but still link down;

    3、The HPD signal  has connect from the HDMI connector to the FPGA,because HMDI can link up via pin strap mode for 1080P or 4k@30hz,

    4、OE pin connect to cpld,so OE pin pull high 30ms after power on;

    • This project consists of two board cards.A piece of the board use a piece of TMDS181 and FPGA for HMDI Source,Another

      board use a piece of TMDS181 and FPGA for HMDI Sink。

    • If the source card and sink card configure via pin strap mode,they can be linked up in 1080P or 4k@30hz。However,the source card configures via I2C
    • mode,and the sink card still configures via pin strap mode,they can't link up.
    • Do you have any suggestion why TMDS181 don't have output via I2C mode?

    Block Diagram of TMDS181.pdfTMDS181-SOURCE.pdfTMDS181-SINK.pdf

  • Hi,

    1. In the register dump, I see the TMDS_CLK_RATIO_STATUS being set to 1. TMDS_CLK_RATIO_STATUS only sets to 1 for HDMI2.0, it needs to be set to 0 for HDMI1.4 or lower operating speed. Are you setting the TMDS_CLK_RATIO_STATUS bit correctly between the HDM1.4 and 2.0?

    2. Are you setting the TX_TEMR_SEL bits correctly between the HDMI1.4 and 2.0?

    Data rate (DR) > 3.4 Gbps – 75 to 150 Ω differential near end termination -> HDMI2.0

    2 Gbps > DR < 3.4 Gbps – 150 to 300 Ω differential near end termination -> HDMI1.4

    DR < 2 Gbps – no termination -> HDMI1.4

    3. Can you probe the source card TMDS181 clock output when the TMDS181 is in I2C mode?

    Thanks
    David

  • Hi,David

    1、I've tried to set the TMDS_CLK_RATIO_STATUS for HDMI1.4,but still link down;

    2、The TX_TEMR_SEL bits of  the register has been seted to 01 for HDMI1.4,but still link down;

    3、FPGA of INPUT CARD detected a clock signal in I2C mode。

    Do you have anyother idea to analyse and  solve the problem?   or  Are there any other problems with my hardware circuit design?

    How to configure the hardware circuit of  TMDS181 If the Output Card  can linkup at 4k@60hz via PIN starp mode?   and  How to configure the hardware circuit of  TMDS181 If the HDMI can display  between 1080P、4k@30hz and 4k @60hz?

    GT status
    ---------
    RX reference clock frequency: 148498432 Hz
    DRU reference clock frequency: 125000000 Hz
    RX: CPLL
    RX state: ready
    
    CPLL settings
    -------------
    M : 1 - N1 : 5 - N2 : 4 - D : 4
    
    RX MMCM settings
    -------------
    Mult : 8 - Div : 1 - Clk0Div : 16 - Clk1Div : 8 - Clk2Div : 16
    0x0 0x54
    0x1 0x4d
    0x2 0x44
    0x3 0x53
    0x4 0x31
    0x5 0x38
    0x6 0x31
    0x7 0x20
    0x8 0x1
    0x9 0x2
    0xa 0x33
    0xb 0x8
    0xc 0x60
    0xd 0x0
    0xe 0x0
    0xf 0xf
    0x10 0x0
    0x11 0x0
    0x12 0x0
    0x13 0x0
    0x14 0x0
    0x15 0x0
    0x16 0x0
    0x17 0x30
    0x18 0x0
    0x19 0x0
    0x1a 0x0
    0x1b 0x0
    0x1c 0x0
    0x1d 0x0
    0x1e 0x0
    0x1f 0x0
    0x20 0xa
    0x21 0x0
    0x22 0x0
    0x23 0x0
    0x24 0x0
    0x25 0x0
    0x26 0x0
    0x27 0x0
    0x28 0x0
    0x29 0x0
    0x2a 0x0
    0x2b 0x0
    0x2c 0x0
    0x2d 0x0
    0x2e 0x0
    0x2f 0x0
    0x30 0x0
    0x31 0x0
    0x32 0x0
    0x33 0x0
    0x34 0x0
    0x35 0x0
    0x36 0x0
    0x37 0x0
    0x38 0x0
    0x39 0x0
    0x3a 0x0
    0x3b 0x0
    0x3c 0x0
    0x3d 0x0
    0x3e 0x0
    0x3f 0x0
    0x40 0x0
    0x41 0x0
    0x42 0x0
    0x43 0x0
    0x44 0x0
    0x45 0x0
    0x46 0x0
    0x47 0x0
    0x48 0x0
    0x49 0x0
    0x4a 0x0
    0x4b 0x0
    0x4c 0x0
    0x4d 0x0
    0x4e 0x0
    0x4f 0x0
    0x50 0x0
    0x51 0x0
    0x52 0x0
    0x53 0x0
    0x54 0x0
    0x55 0x0
    0x56 0x0
    0x57 0x0
    0x58 0x0
    0x59 0x0
    0x5a 0x0
    0x5b 0x0
    0x5c 0x0
    0x5d 0x0
    0x5e 0x0
    0x5f 0x0
    0x60 0x0
    0x61 0x0
    0x62 0x0
    0x63 0x0
    0x64 0x0
    0x65 0x0
    0x66 0x0
    0x67 0x0
    0x68 0x0
    0x69 0x0
    0x6a 0x0
    0x6b 0x0
    0x6c 0x0
    0x6d 0x0
    0x6e 0x0
    0x6f 0x0
    0x70 0x0
    0x71 0x0
    0x72 0x0
    0x73 0x0
    0x74 0x0
    0x75 0x0
    0x76 0x0
    0x77 0x0
    0x78 0x0
    0x79 0x0
    0x7a 0x0
    0x7b 0x0
    0x7c 0x0
    0x7d 0x0
    0x7e 0x0
    0x7f 0x0
    0x80 0x0
    0x81 0x0
    0x82 0x0
    0x83 0x0
    0x84 0x0
    0x85 0x0
    0x86 0x0
    0x87 0x0
    0x88 0x0
    0x89 0x0
    0x8a 0x0
    0x8b 0x0
    0x8c 0x0
    0x8d 0x0
    0x8e 0x0
    0x8f 0x0
    0x90 0x0
    0x91 0x0
    0x92 0x0
    0x93 0x0
    0x94 0x0
    0x95 0x0
    0x96 0x0
    0x97 0x0
    0x98 0x0
    0x99 0x0
    0x9a 0x0
    0x9b 0x0
    0x9c 0x0
    0x9d 0x0
    0x9e 0x0
    0x9f 0x0
    0xa0 0x0
    0xa1 0x0
    0xa2 0x0
    0xa3 0x0
    0xa4 0x0
    0xa5 0x0
    0xa6 0x0
    0xa7 0x0
    0xa8 0x0
    0xa9 0x0
    0xaa 0x0
    0xab 0x0
    0xac 0x0
    0xad 0x0
    0xae 0x0
    0xaf 0x0
    0xb0 0x0
    0xb1 0x0
    0xb2 0x0
    0xb3 0x0
    0xb4 0x0
    0xb5 0x0
    0xb6 0x0
    0xb7 0x0
    0xb8 0x0
    0xb9 0x0
    0xba 0x0
    0xbb 0x0
    0xbc 0x0
    0xbd 0x0
    0xbe 0x0
    0xbf 0x0
    0xc0 0x0
    0xc1 0x0
    0xc2 0x0
    0xc3 0x0
    0xc4 0x0
    0xc5 0x0
    0xc6 0x0
    0xc7 0x0
    0xc8 0x0
    0xc9 0x0
    0xca 0x0
    0xcb 0x0
    0xcc 0x0
    0xcd 0x0
    0xce 0x0
    0xcf 0x0
    0xd0 0x0
    0xd1 0x0
    0xd2 0x0
    0xd3 0x0
    0xd4 0x0
    0xd5 0x0
    0xd6 0x0
    0xd7 0x0
    0xd8 0x0
    0xd9 0x0
    0xda 0x0
    0xdb 0x0
    0xdc 0x0
    0xdd 0x0
    0xde 0x0
    0xdf 0x0
    0xe0 0x0
    0xe1 0x0
    0xe2 0x0
    0xe3 0x0
    0xe4 0x0
    0xe5 0x0
    0xe6 0x0
    0xe7 0x0
    0xe8 0x0
    0xe9 0x0
    0xea 0x0
    0xeb 0x0
    0xec 0x0
    0xed 0x0
    0xee 0x0
    0xef 0x0
    0xf0 0x0
    0xf1 0x0
    0xf2 0x0
    0xf3 0x0
    0xf4 0x0
    0xf5 0x0
    0xf6 0x0
    0xf7 0x0
    0xf8 0x0
    0xf9 0x0
    0xfa 0x0
    0xfb 0x0
    0xfc 0x0
    0xfd 0x0
    0xfe 0x0
    0xff 0x0
    [END]
    ~ # 

  • Hi,

    On the source side, if you only set the I2C_EN pin to high, leave TERM = NC, and don't do any I2C read or write, are you able to get the link up?

    Please follow the design example in Figure 36, the key is to make sure the TMDS181 SDA_SNK and SCL_SNK connected to the DDC bus so the TMDS181 can snoop the bus correctly and set the TMDS_CLK_RATIO_STATUS bit correctly between the1080p, 4k@30, and 4k@60. The TX_TERM_SEL needs to be set to NC so it can automatically set to the right termination based on the data rate.

    Thanks
    David

  • Hi,David

      Thanks for your reply in these days?

      I found out the cause of the problem that CPU  don't configure  the register bit of video source of FPGA .Now the project can display to1080p  and 4k@60hz.  SDA_SNK and SCL_SNK need to be connected to the DDC bus between the FPGA and the HDMI connector .

    I have anyother questions that need your reply?

    1、how to configure PIN 17 ( SIG_EN) of TMDS181 IN PIN strap mode and i2c mode? 

    2、Does TMDS181  need to  pull up 50 Ω termination resistor  in DC-coupled mode (sink side  or source side)?

  • Hi,

    Thanks for the update.

    1. I would leave SIG_EN pin pulled low to disable the clock detector circuit in the pin-strap mode. In the I2C mode, pin 17 is overwritten by register 0x09 bit 4 which is disabling the clock detector circuit by default.

    2. I think you are referring to the TMDS181 output? For the TMDS181 output and DC coupled mode, then there is no need to have the external 50ohm termination to 3.3v as long as the sink already internally has the termination.

    Thanks

    David

  • Hi,David

      Thank you for your help in these days !