Part Number: TMDS181
Hello team,
My customer is using the TMDS181 and has some questions. Could you please help with it? Thank you!
When soldering the device in their factory, they may connect the RXin0+ to the GND, but they enabled the adaptive EQ, so the eye height is ok when the RXin0+ is connected to the GND, We want to find the bad board by reading the register.
I think there are two ways:
1. Disable the adaptive EQ and fix the EQ value, read back the eye. We just need to set the 0xa0's bit5 to 0. Is that right?
2. Or we can keep the adaptive EQ function and read back the CTLE value. But I can't find the CTLE value register in the DS. Can you send me the register to read the CTLE value?
Thank you!