This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1002: Setting for using TUSB1002?

Part Number: TUSB1002
Other Parts Discussed in Thread: , TUSB522P,

Hi, I am going to use TUSB1002 for my usb 3.2 device.

I have 4 questions for using this. Please help me.

-----------------------------------------------------------

Tusb1002 has too many options for setting.

But there is no pcb area for put pin header for options like TUSB1002EVM.(EQ1, EQ2, CF1, CF2, ..etc)

I am using this TUSB1002 first time, so I have no idea about how these settings wil effect USB Signals.

-----------------------------------------------------------------------------------------------------------------

1. What do you think about make all the pins for floating and put NC resistor for later tuning options?

Are making Floating these pins are kind of default mode?

-----------------------------------------------------------

2. I have another question about mode pin.

Mode 0 = Basic Redriver mode

Mode F = USB 3.2 Dual channel operation.

Could you tell me what is different between Basic Redriver mode and Dual channel operation?

---------------------------------------------

3. I have used TSUB522P before.

When I used this, No accoupling capacitors are placed on the RX2P and RX2N pins

because it is assumed the device downstream of the TUSB522P will have ac-coupling capacitors on its transmitter as defined by the USB 3.1 specification. 

But In the datasheet TUSB1002, there says like below.

Is this mean I don't have to put ac coupling capacitor?

Or If I put 330nF and 220k Resistors as options, how does it will effect?

---------------------------------------------------

4. If I use TUSB522P for USB3.2 Devices, won't this work properly?

5. Can I tie EN pin to VCC?

Thanks.