This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team
Would you provide any explanation materials which show required limitation of S-parameter on transmission line for SERDES?
A customer found a documentation for design of FPD-Link III system as shown in below, but the documentation don't describe such limitation.
How to design a FPD-Link III system using DS90UB953-Q1 and DS90UB954-Q1
I think the customer want to calculate maximum length of cable or allowable loss in a connector from the limitation and cable loss.
Your cooperation will be appreciated.
Best Regards, Taki
Hi Takigasaki-san,
Table 227 in the 954 datasheet has the channel requirements.
Best,
Jiashow
Hi Jiashow-san
Thank you for your reply.
One of the customer's assumption is to use 953A and 960.
In this case, I think that table 7-6 and 7-7 in 960 datasheet show the channel requirements also.
Is my understanding correct?
Best Regards, Taki