As per our requirement, our connection is as follows.
10G sfp signals from PORT_MAIN are connected to HS of TLK10031. LS signals of PORT_MAIN TLK10031 are connected to MUX, and can be switched to any of the devices( say LINK A, LINK B are connected to LS side of another device). Again at the HS signals of corresponding devices are connected to the SFP.
Our doubt is, whether we want to connect LS_OK_IN_A (B10 pin) of PORT_MAIN TLK10031, to be connected to the LS_OK_OUT_A (D9 pin) of LINK A TLK10031 & LINK B TLK10031 via mux.
LINK_OK_OUT_A (D9 pin) of PORT_MAIN TLK10031, to be connected to the LS_OK_IN_A (B10 Pin) of LINK A TLK10031 & LINK B TLK10031 via mux.