This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10031: TLK10031 -LS_OK_IN_A (B10 Pin) & LS_OK_OUT_A (D9 Pin) connection

Part Number: TLK10031

As per our requirement, our connection is as follows.

10G sfp signals from PORT_MAIN are connected to HS of TLK10031. LS signals of PORT_MAIN TLK10031 are connected to MUX, and can be switched to any of the devices( say LINK A, LINK B are connected to LS side of another device). Again at the HS signals of corresponding devices are connected to the SFP.

Our doubt is, whether we want to connect  LS_OK_IN_A  (B10 pin) of PORT_MAIN  TLK10031, to be connected to the LS_OK_OUT_A (D9 pin) of LINK A  TLK10031  & LINK B TLK10031 via mux.

LINK_OK_OUT_A  (D9 pin) of PORT_MAIN  TLK10031, to be connected to the LS_OK_IN_A (B10 Pin) of LINK A  TLK10031  & LINK B TLK10031 via mux.