Part Number: SN65LVPE501
Hi Team, just for quick clarification about PCIe repeater chip Rx Detect function.
Does the part-turn off (Set to HiZ) it's receiver terminations if it does not detect a receiver on a transmitter?
Thank you very much.
-Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVPE501
Hi Team, just for quick clarification about PCIe repeater chip Rx Detect function.
Does the part-turn off (Set to HiZ) it's receiver terminations if it does not detect a receiver on a transmitter?
Thank you very much.
-Mark
The response from Nasser does not answer the question. It gives two impedances presumably for two situations but does not say when the part uses a those impedances. The data sheet says the if en_rxd is high when rst goes high and is high the part will perform the rxdetect function on both of its transmitters until it detects a receiver on both transmitters. It never really says if the rxdetect function has an effect of the receiver impedance. The data sheet seems to indicate that only rx_en has an affect on the receiver impedance impedance. It would be most beneficial if the presence of a receiver would switch the associated transmitters impedance fro High-Z to proper termination.
Hi Mark and Carl,
Hope i can answer the question clearly. On power up - when enabled through RX Detect pin - device sends out out RX detect pulses on its transmitter toward the end point.
a). If it detects a 20K ohm or higher on its transmitter - end point RX termination - it assumes there is not termination on its output. In this case, device RX termination - seen typically by the CPU - is also high impedance(>20K ohm).
b). On the other hand if it detects 60-ohm +/-15% on its transmitter, then it assumes there is a valid termination. In this case, device turns on its own RX 50-ohm termination. This signals the CPU to start PCIe protocol negotiations.
Regards,, Nasser
Thank you! This latest reply does answer the question and even gives the hoped for answer. I am guessing that the device will not detect if the far end receiver termination goes to >20k. It would be difficult to determine teh loss of termination once the system is passing traffic.