Hi Team, just for quick clarification about PCIe repeater chip Rx Detect function.
Does the part-turn off (Set to HiZ) it's receiver terminations if it does not detect a receiver on a transmitter?
Thank you very much.
-Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team, just for quick clarification about PCIe repeater chip Rx Detect function.
Does the part-turn off (Set to HiZ) it's receiver terminations if it does not detect a receiver on a transmitter?
Thank you very much.
-Mark
Hi Mark,
PCIe specifies high impedance as greater than about 20K-Ohm. When terminated it is specified as 60-ohm +/-15%. So there is a big jump.
Regards,, Nasser
The response from Nasser does not answer the question. It gives two impedances presumably for two situations but does not say when the part uses a those impedances. The data sheet says the if en_rxd is high when rst goes high and is high the part will perform the rxdetect function on both of its transmitters until it detects a receiver on both transmitters. It never really says if the rxdetect function has an effect of the receiver impedance. The data sheet seems to indicate that only rx_en has an affect on the receiver impedance impedance. It would be most beneficial if the presence of a receiver would switch the associated transmitters impedance fro High-Z to proper termination.
Hi Mark and Carl,
Hope i can answer the question clearly. On power up - when enabled through RX Detect pin - device sends out out RX detect pulses on its transmitter toward the end point.
a). If it detects a 20K ohm or higher on its transmitter - end point RX termination - it assumes there is not termination on its output. In this case, device RX termination - seen typically by the CPU - is also high impedance(>20K ohm).
b). On the other hand if it detects 60-ohm +/-15% on its transmitter, then it assumes there is a valid termination. In this case, device turns on its own RX 50-ohm termination. This signals the CPU to start PCIe protocol negotiations.
Regards,, Nasser
Thank you! This latest reply does answer the question and even gives the hoped for answer. I am guessing that the device will not detect if the far end receiver termination goes to >20k. It would be difficult to determine teh loss of termination once the system is passing traffic.