This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
team,
The target is to prevent leakage from both directions when the device is disabled no matter 3.3V or 1.8V comes earlier.
Better to have small package and less pins for PCB space consideration.
Do we have simplier device other than PCA9306 (maybe save the VREF1/VREF2 pins)?
Thanks
Max
It is I2C. Need to support the maximum data rate 3-4MHz. The key consideration is to prevent the leakage from Side A-B and also B-A in case the pull-up power rail is not active at the same time.
A direction-controlled translator would not work with I²C.
Translators like LSF and TXS leak through the power supply pins. I guess it is not possible to pull the LSF's EN pin low?
Is it OK to prevent the leakage if we tie the EN pin to the power rail that rises later? Or may be if we connect the EN to MCU to draw it low.
I mean, if we disable the device, but the power rail on one side raise earlier than the other, could any of the device could stop the leakage between the 2 power supplies?
Do you know which supply rises first?
If EN is pulled low, it must be done actively with an open-drain driver; see Using the Enable Pin with the LSF Family.