This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does TI have any SerDes chips which will comply with EN60601 medical standards?
I'd like to know if there are any SerDes chips that are medical grade? or example, is the DS90UB913 medical grade? i'm checking if DS90UB913 can be used.
who can i contact here in Europe that could help to see if this chip can be certified later for EN60601?
Hi Hamzeh,
I do have the same question from the thread you shared.
I'd like to clarify if the SerDes is qualified for Safety-Related Certifications such as the following?
For example, the datasheet of ISO7821LLS specifically mentions this type of certifications. Are there SerDes chips which also have this indications?
-Renelson
Hello Renelson,
Can you please cpecify what are you looking to achieve at the system level? Is this is something related to isolation?
Hello Renelson,
FPD-Link is not an isolated technology so I don’t think that would be applicable. Nevertheless, below you can see the topology we suggest for medical application, which should work for you as well!