This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
we are using a DP83822I with a ST Controller. When we set the PHY to 10Base-Tx there are no Problems and we can use a TCP server loop back example from ST.
When we select 100Base-Tx or Autonegaotiation the PHY can not get a stable link to the ethernet switch. The link cycles with up time for about 500ms and down time for about 1s.
When we take a look at the registers 0x10 the bit 1 (speed status) changes from 0 to 1 and back. With automdix we get the following Register entries:
Here is the schematic of the DP83822I interface:
We have done some measurement of the signals between the eternet inductor and the PHY showing a link puls, communication in autonegatiation mode and a autonegotiation paket:
Has someone the same problems with the PHY?
Regards Mario
Hi Rob,
we have tested three different Switches
- HP procurcve 4104gl
- NETGEAR FS105
- bintec R1200
On all switches the same problem.
Regards Mario
Hi,
the Problem is solved.
The chrystal was not as stable as needed.
Regards Mario