This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9539: I2C input rise and fall time for FAST MODE

Part Number: TCA9539


The minimal input rise time is 20 ns and the minimal input fall time is 20 x (VCC / 5.5 V) ns.

Are those specifications really correct for the SDA and SCL input terminals?

In the I2C-bus Specification, the minimal rise and fall time is the specification for the output terminals and the bus lines, and it does not seem to be the specification for the input terminals.

I2C-bus Specification, Version 6.0, 4th of April 2014
http://cache.nxp.com/documents/user_manual/UM10204.pdf

On our customer board, no problems have occurred but the minimal rise and fall time is approximately 2.4 ns. Is this minimal time allowed?

Best regards,

Daisuke